web counter

Designing Application-Specific Integrated Circuits

Published: 07 March 2025 | Last Updated: 07 March 20252682
This article explores the design process, benefits, and roles of Application-Specific Integrated Circuits in enhancing performance and efficiency in embedded systems.

General-purpose processors are designed to handle a wide range of tasks, which makes them versatile but less efficient for specific applications. They face several challenges when compared to Application-Specific Integrated Circuits (ASICs),

What is an ASIC?

An Application-Specific Integrated Circuit is a type of circuit custom-designed to perform a specific function or set of functions. They provide high performance and efficiency for specialized applications. Despite the advantages, ASICs face several challenges, including high initial costs and long development cycles, making them primarily suitable for high-volume production.

Designing Application-Specific Integrated Circuits

Design complexity is a primary challenge that involves increased verification efforts, power planning, and advanced packaging. Various steps in designing an ASIC are depicted in Fig. 1. This article provides a comprehensive overview of the ASIC design process, detailing the various steps from concept to production.

The ASIC design cycle is divided into frontend and backend domains, similar to software development. The front-end design deals with the visible aspects of the chip, such as its functionality and behavior. Backend design handles the hidden, physical aspects of the chip, such as layout and manufacturability.

wps1.jpg 

Fig. 1 Design flow of application-specific integrated circuits Source: MDPI

Step 1: System Specification

It involves gathering information from stakeholders regarding the circuit's electrical and functional requirements. All the specifications, including I/O pins, functionality, power, dimensions, and how the chip should function under various scenarios, including environmental conditions, power consumption, and performance requirements, are all examined.

Step 2: Architectural Design

An outline of the chip's overall structure comprising a high-level block diagram and interconnect for every module is created.

Step 3: RTL Design

It is the step in the ASIC design flow where high-level behavioral descriptions of a system, often written in C, C++, or MATLAB, are automatically converted into register transfer level (RTL) code in Verilog or VHDL. RTL bridges the gap between high-level functional specifications and the physical implementation.

Step 4: Functional Verification

After the design has been implemented in HDL, simulations must be performed to verify that the circuit satisfies the required electrical specifications. It employs test benches like universal verification methodology (UVM), which are automated test protocols used to verify functionality and to identify and fix bugs before synthesis.

Step 5: Synthesis

During the logic synthesis phase, the RTL code is converted into a gate-level netlist that can be used for physical implementation. Converting RTL code into physical components collectively known as standard cells that are pre-designed building blocks such as logic gates, flip-flops, multiplexers, and buffers. Multiple optimizations are applied to enhance the final circuit's speed, area, and power efficiency.

Step 6: Formal Verification

Formal verification detects that a design adheres to its specifications and operates correctly under all possible conditions. Unlike functional verification, it uses mathematical techniques to examine all execution paths.

Step 7: Floor Planninig

The first step in physical design is where the core area of the chip is divided among functional blocks such as logic elements, memory structures, and I/O interfaces. The goal is to optimize chip area usage and performance while minimizing interconnect delays.

Step 8: Placement and Routing

The electronic design automation (EDA) tool places and routes standard cells and hardware within the allocated floorplan. Placement ensures that timing constraints are met and minimizes wire lengths to reduce delays. It is an essential step, as poor placement can lead to increased area, performance degradation, increased power consumption, and reduced reliability.

Step 9: Clock Tree Synthesis (CTS) and Timing Analysis

CTS is a step in physical design where the EDA tool generates a clock distribution network. Every sequential circuit inside the chip requires a clock. CTS ensures proper timing and synchronization; the clock path's length is important because longer paths introduce more delay, which can lead to timing violations.

Step 10: Physical Verification and Signoff

The signoff stage is the final verification step commonly used to ensure the design is ready for manufacturing. During this stage, a series of analyses are conducted.

● Layout Versus Schematic (LVS): Verifies that the physical layout of the circuit matches the original schematic or netlist generated during logical synthesis.

● Voltage Drop (IR Drop) Analysis: Assesses voltage consistency across power distribution networks.

● Static Timing Analysis (STA): Evaluate whether the design meets all timing constraints across all paths, such as setup and hold times.

● Design Rule Checking (DRC): It is part of physical verification that ensures that the final layout adheres to the manufacturing rules provided by the foundry in the Process Design Kit (PDK).

Once all the ASIC design process steps are completed, the layout's geometric files are exported in GDSII (Graphic Data System II) format, known as tapeout. This file format is essential for transferring the physical layout data to the semiconductor foundry for manufacturing.

Step 11: ECO & Chip Fabrication

The fabrication of a chip in a foundry is a highly intricate process that involves multiple stages to transform the design into a physically integrated circuit. The entire fabrication process is extremely complicated and involves numerous steps.

Step 12: Packaging and Testing

After fabrication, they are packaged to protect them from environmental factors and provide electrical connections. Packaged ASICs undergo testing to ensure functionality and performance.

Step 13: Post Silicon Validation

This step ensures that the fabricated ASIC meets all functional, performance, and reliability specifications in real-world conditions. Functional testing with actual workloads or application scenarios is carried out.

Step 14: Final Chip

Once all tests and validations are complete, the final chip is ready for mass production or deployment. At this stage, the ASIC is considered fully verified, robust, and optimized for its specific purpose.

The ASIC design process involves various validation steps to meet the desired specifications and performance requirements.

Summarizing the Key Points

● ASICs enhance performance and efficiency for specific tasks, overcoming the limitations of general-purpose processors despite their higher initial costs.

● The ASIC design process is complex, involving multiple stages like system specification, RTL design, and functional verification.

● This complex design flow ensures that the circuit meets functional and performance requirements for specific applications.

Reference

Franck, L. D., Ginja, G. A., Carmo, J. P., Afonso, J. A., & Luppe, M. (2023b). Custom ASIC design for SHA-256 using Open-Source tools. Computers, 13(1), 9. https://doi.org/10.3390/computers13010009

Mendez, T., Parupudi, T., K, V. K., & Nayak, S. G. (2024b). Development of Power-Delay Product optimized ASIC-Based computational unit for medical image compression. Technologies, 12(8), 121. https://doi.org/10.3390/technologies12080121

The Octet Institute. ASIC Design Flow | How a chip is designed?? [Video]. YouTube. https://www.youtube.com/watch?v=1CFhcBH52Rc

Rakesh Kumar, Ph.D.

Rakesh Kumar holds a Ph.D. in electrical engineering with a specialization in power electronics. He is a Senior member of the IEEE Power Electronics Society, Class of 2021. He is currently associated with the KPR Institute of Engineering and Technology, India. He writes high-quality, long-form technical articles on power electronics for B2B electronics platforms. Feel free to reach out to him at rakesh.a@ieee.org!

Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242991

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255874

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20262387

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261260

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 20261144

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More